Tool/software:
Hi, this is Gilhwan Cha.
A buck-boost rail grounding and short-circuit issue occurred.
It was in use on a custom board, and the decap configuration utilised the same decap as the EVK.
The problem arose when the Vsys pin and BUBO pin were shorted.
Naturally, this short should not occur, but it happened accidentally for about one second.
Subsequently, when power is applied, heat is generated from the BQ25190.
Furthermore, the BBSW1 and BBSW2 pins are shorted to GND.
Additionally, when the 5V supply is applied, IN is detected as 4.75V.
Thanks.