UCC28750: Requesting for a Home automation circuit design as per industry standard.

Part Number: UCC28750
Other Parts Discussed in Thread: UCC28742

Tool/software:

Hi to all.

i want to develop a home automation product. so for that i use hilink 5v smps as an input from 230v to 5v. but apart from that what are the input protection circuits i can use for ac input. as wll as for manual switching point, for mcu, for relay what type of protection circuits i can use . please guide me as per industry standards. if you have any circuit which can convert 230v input to 5v, 1A. then i can directly use it with all protection circuit. Plz guide me on the design part.

  • Hi Smruti,

    I am not sure which standards you need to adhere to, but PMP40487 looks like a good starting point.  This is using the UCC28742 which would be more efficient than the UCC28750. Here is a WEBENCH design to get you started with the UCC287502.

    I hope this answers your question.