This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1686: Power Switch Selection Discuss

Part Number: TPS1686
Other Parts Discussed in Thread: TPS25984, TPS1685, LM5067

Tool/software:

Hi TIer

My customer want to choose two power switch or efuse. Could you help me check and give some suggestion? Thank you very much.

  1. -5V (maximum -6V) 3A , need over current over voltage protect , this is power rail switch.
    1. I see we don’t have -5V 3A switch, right? If not ,which one is suitable for this socket?
  2. Large than 30V , large than 20A power switch ,protect.
    1. TPS1686 can support it? Do you have more suggestion?

Thank you very much.