Other Parts Discussed in Thread: TPS61020EVM-025
Tool/software:
I am testing the TPS61027DRCR using the TPS61020EVM-025 evaluation board. The output is set to 5 V and the input supply is 3.3V
When applying a load transient from 100 mA to 1 A using a DC electronic load in pulse mode, the output voltage drops (Nearly 3V)significantly and does not maintain regulation.