Tool/software:
Hi, I have had this two-layer PCB layout running fine for a year or so, but the most recent batch of PCBs has a problem where it goes into an unstable mode:
- the STAT1 LED flashes briefly once every two seconds
- BTST net is as shown on the trace during the charging phase (which cycles on and off)
Charging li-ion at a target of 16.8v, using a 21V 10W solar panel, at 1A max current. While the battery is low voltage and the charge current is high, everything seems OK, until some point (which varies) during charge when it becomes unstable.
I am OK to make modifications to the PCB layout if needed, but would need to know the source of the problem so I can change the appropriate section. Or even another component I can retrofit to existing PCBs to ensure stability.
Gerber attached.
Unstable on BTST, approx 16v at peak.