Tool/software:
Dear TI, forum readers,
I want to connect LEDs to STAT1 and STAT2 pins of the BQ25185.
There is a table in the datasheet of the BQ25185 (page 18/19): section 8.3.10 Status Pins describing the behaviour of the status pins.
However, when there is no VIN present, I would expect the STAT1 and STAT2 pins to be off/low, otherwise they would drain the battery, right?
Is this the behaviour of the BQ25185? This is not clear from the BQ25185 datasheet.
Any other things I need to keep in mind when connecting STAT1 and STAT2 to LEDs?
Regards
Thomas.