LMR60420: High failure rate in production using a reference design

Part Number: LMR60420

Tool/software:

I am having issues with the use of the LMR604205RAKR in my design. Almost half of a batch of 20 will exhibit a short on the input of the IC causing it to emit the magic smoke if you give it more than an amp or so. The design is very simple and basically follows one of the examples given in the datasheet. The only addition is an SMF28A for input protection which I have checked the polarity of.

Some units will fail like this immediately, others some time after they are assembled, which is making quality control very difficult. They are being tested at 24Vin with a good lab power supply current limited to 100mA. No load is on the output when they are tested.

My best guess is some kind of issue with the soldering, but I can't think of a bridged connection that would cause the chip itself to burn up.

Schematic for your consideration: