Tool/software:
In the "EVM User's Guide: TPS55287Q1EVM-085," there is an evaluation module schematic and Bill of Materials.
The schematic shows C21 as a 0.22 μF capacitor. The BOM lists it as a 0.1 μF capacitor.
I am trying to decide if:
(1) It was easier to use a 0.1uF because there were others used on the board.
(2) The schematic is wrong.
(3) The BOM is wrong.
(4) During testing, it was determined C21 should be 0.22uF or vice versa it should be a 0.1uF.
I understand the application of the capacitor in the circuit, but I am second-guessing if testing found one value more productive over the other.
Thoughts?
Thank you.