Tool/software:
Hello,
On a design with a UCD90160A, I have an unexpected behaviour. The problem occurs approximately once on twenty power-up sequences
Durring power-up phase, an interruptions occured on SMB_Alert#.
After having an interruption on SMB_Alert#, the STATUS_WORD(0x79) register is stuck at 0x0108.
0x0108 correspond to an unknown fault and an input undervoltage condition.
The input voltage is stable.
Writting the CLEAR command 0x03 don't reset the register. (Using both our microcontroller or TI probe)
In addition, writting a soft reset command 0xDB don't reset the devices, and STATUS_WORD keep is 0x0108 value
Does the soft reset command is supported?
Thanks,
Robin