Tool/software:
I am looking at using the LM60440 in an application where we are only going to have a Peltier TEC module attached directly to the output of the power supply. Maybe I am oversimplifying this - but I am thinking this will essentially be a fixed load and as such, do not expect there to be any transients.
The output of the power supply would be set to 7V and at 7V, I am expecting the Peltier to draw around 3A of current.
For calculating the minimum Cout, I'm using equation (5) in the datasheet, but I'm not sure what I should be using for ΔIout / ΔVout. Should I set ΔIout / ΔVout = 1?
Thanks for your help!