UCC28950: Inquiry Regarding Tmin Setting for UCC28950

Part Number: UCC28950

Tool/software:

Hi,

I am currently implementing and testing a PSFB converter using the UCC28950 chip.

I have a question about the Tmin setting. The datasheet states that Tmin should be set to the minimum duty cycle that allows for ZVS (Zero Voltage Switching) under light-load conditions, but I need a more detailed explanation of this.

Could you please provide any design guidelines on this topic? Also, if you have any reference documents I could review, I would greatly appreciate it.

  • Hello,

     

    Tmin setting determines when the device goes into burst mode.  Burst mode is triggered when the duty cycle/(switching frequency is less) < Tmin. 

     

    In regards to ZVS you need to properly select the shim inductor (Ls) and set the delay timing of the device.  The following will bring you to and application note that discusses how to select Ls and setup the delay timings to achieve ZVS.

    https://www.ti.com/lit/pdf/slua560

    Regards,

  • I understand that the RTMIN resistor sets the minimum on-time (tMIN) before entering burst mode. However, I'd like to know the rationale for choosing a specific value for this minimum on-time, or if you could point me to any relevant documentation

  • Hello,

     

    The only information in regards to this is setting Tmin in the data sheet.

     

    Originally the purpose of this was to enable light load burst to improve light load efficiency to reduce losses caused by driving the H Bridge FETs; as well as, the FETs switches losses.

     

    Most of the customer that I work with set this set the Tmin to the lowest setting possible to avoid audible noise.

     

    Regards,