Tool/software:
in LMR36506 Datasheet, I can calculate the Iq_vin like this Fomula.
I use Vin = 40V. I can't Find the That Spec in Datasheet. There are Only Vin 13.5V & 24V Spec.
So Can you let me know about That Spec in Vin = 40V.
Tool/software:
in LMR36506 Datasheet, I can calculate the Iq_vin like this Fomula.
I use Vin = 40V. I can't Find the That Spec in Datasheet. There are Only Vin 13.5V & 24V Spec.
So Can you let me know about That Spec in Vin = 40V.
Hi JinYong,
If you are using adjustable output, Ibias is drawn internally from Vin and it shows up in Iq. Unfortunately, we do not have a spec for Iq at Vin = 40V but, looking at IQ_13p5_Adj and IQ_24p0_Adj, there does not seem to be much difference with Vin. So you can consider the same estimate, 22 uA (or +20% for margin), for Iq.
Now, if EN is connected using a resistor divider to Vin, it will draw a current I_EN = Vin/(sum of enable resistors). If it is directly connected to Vin, the leakage current would be in nA and negligible
When using adjustable output, the current taken by feedback resistors also comes into play. This can be calculated as I_FB = Vout/(sum of feedback resistors).
Finally, you can estimate Iq_VIN = Iq + I_EN + I_FB*Vout/(eff * Vin)
Regards,
Niranjan