LMR36506: Recommended device that meets the spec

Part Number: LMR36506
Other Parts Discussed in Thread: LMR54406, LMR50410, LMR51606

Tool/software:

Hello team,

Could you introduce suitable devices that meet below specs? LMR36506 was actually best fit but customer can't use wettable flanks in their manufacturing site so we are looking for other devices.

  • Vin=4V~28V (Abs is higher than 32V)
  • Vout=3.3V
  • Iout=0.3A (max is less than 1A)
  • Support PFM
  • Non wettable flanks 

LMR54406 is one of good options but I want to find others.

Difficulty to find is which device is non wettable flanks or not. First page of LMR36506 datasheet looks only wettable is option but package outline page shows both wettable and non wettable are available. Other Wide-Vin devices are similar situation. I don't know what is true so I'm asking.

Best regards
Koyo