This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG5126: Suitability for 9-28V in 30-60V out 330W boost converter

Part Number: LMG5126
Other Parts Discussed in Thread: LM5171

Tool/software:

I have a design with the specifications below:

Input voltage min: 9V
Input voltage nominial: 20V
Input voltage max: 28V
Input current max: 16.5A @ 20V
Input current >= 5A @ 28V
Input current preferably >=4A @ 12V

Output voltage min: 30V
Output voltage max: 60V
Output current max ~11A @ 30V (330W - losses)
Output current max ~5.5A @ 60V (330W - losses)

The design needs to draw max 330W at 20V, 140W at 28V, preferably >=48W at 12V.
It must be able to provide that power (minus losses) over full output voltage range
The input current limit must be dynamically adjustable via MCU.

Will the LMG5126 be suitable?