This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM33603: Technical Questions About LMZM33603

Part Number: LMZM33603


Tool/software:

I am considering using the LMZM33603 power module in my design. My board has an input supply range of 5–36 V, and I need to regulate it down to 5 V output. Unfortunately, I do not have enough PCB space to implement an isolated converter, so I am planning to use the LMZM33603.

After reviewing the datasheet, I would like to clarify a few technical points:

  1. 5 V Input to 5 V Output Operation

    • From the datasheet, I understand that if the input voltage is 5 V, it is still possible to regulate and obtain 5 V at the output. Is this correct, and are there any limitations or considerations in this operating condition?

  2. Output Filtering Recommendations

    • Since I cannot isolate the power stage, I would like to improve the output quality. Would you recommend adding a π-filter (LC filter) at the output of the module to further reduce ripple and noise? Alternatively, do you have other layout or filtering recommendations for best output performance?

  3. Grounding (AGND vs PGND)

    • I noticed that the module provides analog ground (AGND) and power ground (PGND) pins, which are internally connected. Could you explain the reason for separating them at the pin level?

    • When designing the PCB layout, do you recommend keeping these ground planes separated and then joining them at a single point, or should they be merged into a common ground plane?

    • Would separating them incorrectly cause any performance issues? Do you have a reference layout example that demonstrates the best practice for grounding in this module?

Thank you in advance for your support.

  • Hello,

    1) The device will be in drop out. Please refer to Voltage Dropout in the DS. 

    2) The Buck has an LC on the output, you can increase COUT if additional filtering, if needed. 

    3) Analog ground is for the internal analog circuitry (control circuitry) and Power Ground is for the output stage (Dr, PowerFETs..) 

    Please refer to the layout section of the DS, it provides examples and best layout practices.