Other Parts Discussed in Thread: , TPS55289
Tool/software:
Input voltage: DC 4.8V~18V@45W
Output voltage requires 2 groups:
1.VCC output voltage can be adjusted: 3.3V/5V/10V/12V, 15W
2.VBL: 12~24V can be adjusted within this range, 30W is required
Is the LM5177 a suitable IC?Or do you have any better recommendations?