Tool/software:
Dear TI experts,
Recently I am searching a DCDC which has very low Rth_ja , because the output power dissipation is very high , could you help to recommend one suitable DCDC.
The detail requirement as follows :
1. Input voltage range from 14V to 60V
2. Output voltage is 12V
3. Output current is 2.2A
4. Maximum ambient temperature up to 95℃
5. Automotive grade
To be honest I am worry about the heating and thermal issue , because I don't have enough space for cooling copper of DCDC , so pls. recommend some suitable DCDCs and mark the minimum cooling copper area?
Thanks a lot!