Tool/software:
Hello
I am using the variant of TPS65219 with 07 suffix.
I only need 0.85V (Buck1), 3.3V (Buck2), and 1.8V (LDO2) to power my board.
The question is, do I really have to attatch the required minimum of 30uF as output capacitance to the output of unused Buck3?
I would like to reduce the cost and area by reducing the output capacitance to 10uF, for example.
Best regards