LP5861: LP5861 Powered On State

Part Number: LP5861

Tool/software:

Hi

When LP5861is powered on, the MC data is set to default value, which is 15 mA.

LED current is default when powered on and device enable.

I use LED with max current 10mA.

How to set the initial current value to less than 10mA?