This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2845L-Q1: Flyback design

Part Number: UC2845L-Q1
Other Parts Discussed in Thread: UC3845

Tool/software:

Dear TI team, Now we plan to using UC2845L-Q1 to design a flyback circuit used in automotive.

But I can not found the WB designer for it, so used UC3845 to do the design.

Input Voltage:10~16V

Vout1:170V 0.55A

Vout2:12V 0.5A

Here are my questions:

1. Is UC2845L-Q1 suitable for the output requirement?

2. Is 100khz DCM mode suitable for this application?

3. Does UC2845L-Q1 has the design reference doc?

4. In my applicaiton, shall I remove the primary aux winding, only using Input battery for VCC?

5. What's the design purpose of RZ/DZ/Q1 and R21/D21/C21 in the attached UC3845 WB design file?

WBDesign33.pdf