This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG2100EVM-078: Input capacitance

Part Number: LMG2100EVM-078


Tool/software:

Hello team,

This EVM has 4 pcs of 0.1uF input capacitors, placed close to the VIN pin.

I don't usually see 4pcs of 0.1uF input caps for DCDC converters.

Does GaNFET require more 0.1uF caps than Si based DCDC converters?

Best Regards,
Kei Kuwahara

  • Hi Kuwahara-san, 

    No, there is no set requirement for the total amount of decoupling caps from VIN-GND. This is a value that was chosen for the EVM and has been verified to work without any issue. There is not much difference in decoupling capacitance requirement between Si and GaN. 

    Thanks,

    John