Tool/software:
I need to drive LED 20 Nos with FV = 3 V each. So, the output voltage is 60 V. I adjusted the OVP resistor but LED starts flickering. COMP pin is at 1.2 V. What are the necessary design changes needed to get a Constat current of 1 A
Tool/software:
I need to drive LED 20 Nos with FV = 3 V each. So, the output voltage is 60 V. I adjusted the OVP resistor but LED starts flickering. COMP pin is at 1.2 V. What are the necessary design changes needed to get a Constat current of 1 A
Thanks for your feedback! You mentioned that you adjusted the OVP resistor. May I have your latest schematic with evm board?
Thank you!
BRs
Lucia
The change I made was to add a change resistor R17 to 15k and R7 to 0.2 Ohms(for 1A LED Current) .With that configuration maximum Output voltage was 84 V. Even without that modification when the input of EVM takes about 2.5A at 12V, The fault LED Blinks and LEDs also blinks randomly . OVP is below 1.14V . If i limit the current of the input to 1A . Switching takes place at output side but the current is very low.
Thanks for your feedback. I will look into it and get back to you early next week. Thank you!
BRs
Lucia