This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5852S: creepage and clearance

Part Number: ISO5852S
Other Parts Discussed in Thread: ISO5452, ,

Tool/software:

I reviewed the ISO5852 and see that the datasheet has a confusion, as shared below. Please let me know your thoughts.

 

  1. This ISO5852 is in Standard SOIC-16 package which the minimum distance through air from the drawing inside datasheet between primary-secondary terminals is 7.4mm (which is smaller than 9.1mm requirement).

 

  1. However, the section 7.6 shows the creepage/clearance number of 14.5mm, which cause confusion.