TL7700: TL7700: Estimated allowable error for output pulse duration (tpo)

Part Number: TL7700
Other Parts Discussed in Thread: TPS3842, TPS3808E

Tool/software:

We plan to monitor the power supply with the TL7700.
Could you explain the concept of tpo?
In the data sheet, the tpo section states that when Ct = 0.01uF, it is 0.5 to 1.5 ms.
tpo(typ) = 0.01uF × 10^5 = 1 ms.
From other inquiries, it was noted that there is a ±50% error.
Is this ±50% error due to the IC?
Also, is it acceptable to calculate without including the capacitor's capacitance tolerance or temperature characteristics?