I am using 2 controllers for a 4 phase interleaved pfc. Both controllers are working separately but when I try to sync them by tying the CDR pin to Vref (on both) and driving the RDM pin with a 3.3V pulse that is approx 500nS duration and 180 degrees out of phase with the other channel (as recommended in the data sheet), the 2 controller fail to sync. It appears as though the parts will just run at their separate freqs determined by the RT resistor (75K). I am trying to sync the parts at 145khz so my sync signal is 2x this or 290Khz
Please advise.
Neither channel with sync separately or together
I looked at the signals and they are pretty clean as seen below. The purple is the drain voltage of a single phase (vo=~370V) so the parts regulate etc but donot sync
not