LM61480: LM61480RPHR in Parallel

Part Number: LM61480

Tool/software:

Can two LM61480RPHR ICs be placed in parallel with each other to allow an output that supports higher current than 8A? For example, could two of these ICs be placed in parallel to provide 16A?

  • Hi Jacob,

    Can you share what exactly are your system level specs (i.e. Vin range, Vout, iout, etc.)? 

    LM61480-Q1 doesn't natively support interleaved/parallel function - however, it does have a SYNC pin which you can use to Synchronize two LM61480s and use them in parallel.

    However, do let me know your specs - there are other devices in our portfolio as well which can better suit your application. 

    Thanks,

    Best Regards,

    Taru