Other Parts Discussed in Thread: UCC27532
Tool/software:
Hi team,
My customer is currently designing and testing a FET drive circuit using TI's gate driver "UCC27531DBV" (SOT-23-6 package).
According to the datasheet, the signal inputs (VIN_H/VIN_L) for this device are as follows:
[Excerpt from datasheet]

Inquiry:
Is there any product that is pin-compatible (mounting-compatible) with the UCC27531DBV (SOT-23-6), and also supports input signals (VIN_H, VIN_L) of 5V or higher?
If such a product exists, could you please provide the model number or relevant information?
Best regards,
Kyohei