Other Parts Discussed in Thread: TUSB320,
Tool/software:
Hi team,
My customer is considering connecting a tablet and an MCU (on their custom board) via a Type-C to Type-C cable.
They are planning to configure the devices with the following roles:
- MCU: Data line as Sink, 5V power as Source
- Tablet: Data line as Source, 5V power as Sink
Questions:
-
Is there a PD controller available that supports the above configuration? (Where the roles of Source and Sink are reversed between the data line and the PD line)
-
Regarding the CC controller TUSB320:
I understand that the basic role is determined by connecting external PD/PU resistors to the CC lines on the board.
Is this still the case when operating in DRP (Dual Role Port) mode? -
Referring to the TUSB320, it seems that writing to the MODE_SELECT register at address 0x0A allows switching to DRP mode.
Does this mean that the DRP state can be forcibly set regardless of the resistor values on the CC pins? -
I believe host-device recognition is typically determined at the time of USB connection.
If a PD controller IC is used, is it possible to change roles even after USB startup? (by writing to the above register etc..)
Best regards,
Kyohei