This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36503-Q1: Methods for Surge Protection in 48V Automotive Systems.

Part Number: LMR36503-Q1
Other Parts Discussed in Thread: LMR38010

Tool/software:

I am developing a controller board to be used in a 48V automotive system.

The normal input range of a 48V system is 36V to 54V, making it difficult to select a TVS diode for surge protection.

I'm having trouble finding a suitable TVS diode to use with TI's LMR36503-Q1 DCDC converter.

Could you suggest a suitable TVS diode or other method for surge protection?

Alternatively, if there's a DC/DC converter with an input range of up to 80 V, there seem to be many options for selecting a TVS diode. Do you have any DC/DC converter recommendations?

I want a product that outputs 5V or 3.3V and has a maximum current consumption of 0.3A.