TPS22810: VIN Dependence of the Thermal‑Shutdown Threshold

Part Number: TPS22810

Tool/software:

Hi team,


The datasheet states that the thermal‑shutdown function operates at TJ = 160 °C (VIN = 18 V).

Could you please confirm whether the same threshold applies when VIN = 5 V, or if the threshold changes under this condition?

We measured the device temperature while applying a load current of 2.7 A and calculated TJ = 122.6 °C.

However, when we increased the load current to 2.8 A, thermal shutdown occurred.

This implies that a 0.1 A increase in current results in a temperature rise of more than 30 °C, which raises the question of whether the threshold at VIN = 5 V is set lower than 160 °C.

We would appreciate your clarification on this.

Best regards,
Kazuki Itoh