Tool/software:
In the data sheet of TLV76033DBZR, we can see the "figure16"(Page 8) that seems to show Vout decreasing in the case of Vin>10V.
Does it mean that we need to set up Vin less than 10V?
Tool/software:
In the data sheet of TLV76033DBZR, we can see the "figure16"(Page 8) that seems to show Vout decreasing in the case of Vin>10V.
Does it mean that we need to set up Vin less than 10V?
I'm sorry but let me add the information.
We would like to get 3.3V output.
So my question is "Does it mean that we need to set up Vin less than 10V to get 3.3V output?
Hi Kenta,
This part is rated up to 30V so 10V is not a hard limit threshold. All we need to do is make sure it doesn't hit over 30V and ensure Vin>Vout
Let me know what else you need here :)
Thanks,
Suchit Baliarsingh