TPS56C215: I2C control Vout solution

Part Number: TPS56C215

Tool/software:

Hi Team

do we have any buck converter which vout can be controlled by I2C interface.

below is spec requirement

Vin:12V

Vout: +5V ~ -5V

Iout:1A.

BRs

Brian

  • Hi Brian,

    We may have 17V+ Vin max parts that can do this but most with I2C are higher current parts. I see you have listed 1A output. Is it OK to look at higher current parts for this? If so, I can find some parts. Also when you state -5V, I assume you want the device to run in inverting buck-boost converter fashion which a typical buck can do.

    Thanks,
    Amod