Tool/software:
Dear Sirs and Madams,
I'm running a learning cycle to create a golden image for the BQ27520-G4.
In the first cycle, the Update Status transitioned to 0x02 and the Ra0 Table was updated.
(1)
However, the Ra0x Table was not updated, so two cycles were required, right?
(2)
When creating a golden image, does Ra0 Default require no action?
(3)
The BQ27520-G4 has two tables Ra0 and Ra1.
What should Ra1 Default, Ra1 Table and Ra1x Table be?
Do I need to manually rewrite the Ra0 Table to the Ra1 Table and the Ra0x Table to the Ra1x Table?
Regards,
Masashi