Other Parts Discussed in Thread: TPSM63603
Tool/software:
Hi,
I would like to ask about below.
* I will try to perform operation test by using TLVM13630.
Input condition is 24V + 10% and output is 1.2V(Iout less than 1A) and 3.3V(Iout less than 1A).
(We use two chip.)
At first, as I mentioned above, I will try to use two TLVM13630. However, due to supply issue(we could NOT find TLVM13630 components on web based store such as TI store/digikey/mouser.)
So, I'm considering whether I can use TPSM63603 as replacement.
I have already noticed that main difference is output voltage range and sync function.
Then I have following question.
Q, As I checked datasheet, it seems that electric characteristic is same between TPSM63603 and TLVM13630.
If I use TPSM63603, can I observe SAME result of behavior as case of using TLVM13630 under above input/output condition ?
(In other words, are these same chip only difference is ATE condition ?)
Best Regards,