Other Parts Discussed in Thread: BQ40Z50,
Tool/software:
Hi,
We are using BQ25672 for charging a 4 cell litium ion battery which is have bms Bq40z50.
1. Once our battery get fully depleted it enter into the discharge cut-off. the battery shows 0V in this condition
2. When we connect the battery to the charger, it shows 2.15 V on the terminal and the charge state is trickle charge.
3. The charger continues to charge the battery in trickle charge state for 1 hour and then switch to "not charging" state.
4. The battery does not recover with 2.15 V and 100 mA current.
5. Using a bench supply, I found that battery only recover if we give voltage above 12.6 V
My query is,
1. The data sheet says that voltage during trickle charge is around 2.5 V/ Cell. If I read the register (REG01_Charge_Voltage_Limit Register), it shows value 16.8V detecting the 4S battery. I assume trickle charge voltage should be 2.5 V * 4 = 10 V for 4 cell battery. is this correct ?
2. As battery only recover by applying > 12.6 V then, is there a way to get a fully depleted battery using the charger chip (bq25672)? Any reference note or suggestion will be helpful