Tool/software:
Hi Guys,
I'm attaching a schematic for a 16S standalone BMS. Can you kindly review it ?
1. I've used 9 NTCs in this design. Is there a way to use 18 NTCs ? Can i use two resistors in parallel per thermistor input ?
2. If the BMS is going to be permanently attached to BAT+, do i still need both D1 and D2 ?
3. Is D11 in the DSG circuit used for protection against voltage spikes from regeneration ? Can i remove it ?
Thanks & Regards,
Muki