BQ78350-R1: BQ78350-R1 : CEDV Configuration Clarification

Part Number: BQ78350-R1

Tool/software:

Hello,

I’ve configured the following parameters for the BQ78350-R1:

  • CEDV Gauging Configuration: 0x0012
  • EDV0: 2600 mV
  • EDV1: How should I determine this value?
  • EDV2: How should I determine this value?
  • Overload Current: Must be less than 100 mA
  • Discharge Current Threshold: 20 mA
  • Charge Current Threshold: 20 mA
  • Near Full: 4500 mAh
  • Design Capacity: 4545 mAh
  • Learned FCC (LFCC): 4600 mAh
  • Reserve Capacity: 55 mAh

My goal is to ensure that FCC is updated only when the discharge current is greater than 20 mA and less than 100 mA. Can you confirm if this configuration supports that behavior?

Thank you!