Tool/software:
Hello,
I need to supply an adjustable voltage 1.7-2.7V to a PCB at end-of-line test, 10mA max, 3.6VAbs Max. This will come from an offboard bench supply but I want to dummy-proof accidental setting to higher voltages than this. These are super expensive PCBs.
I'm considering using a tracking LDO to "buffer" the voltage. I want to power the tracking LDO from 3.3V so in no case can it drive to 3.6V.
The TPS7B4255 spec says is can output down to 2.0V, but Figure 6-8 shows it stays linear down to ~1.7V which would be perfect. Can you clarify the datasheet spec or suggest other ideas?
Considering Power Op-Amps as well but it's the same concept, but those seem less happy to drive capacitive loads.
Thanks!