Other Parts Discussed in Thread: TPS40210, LM5575
Tool/software:
We have used the TPS23861 PSE in a number of different product designs, selling a few thousand each year. We have had a number of failures where all 4 ports stop providing POE.
- There is no detection or classification phase.
- The I2C interface is still active although it only appears to be basic digital IO registers that can be read correctly. Vin (0x2E,0x2F) and temperature (0x2C) registers are examples of those that don't provide valid data.
- Voltage is provided from a 12V input, boosted to 50V by a TPS40210, and with the 3.3V supply derived from the 50V with an LM5575. The 3.3V has a UVLO set at about 30V.
- Each port has a protection TVS fitted between Vpwr and Drain similar to the EVM board.
We haven't had any failures where it's only a few ports faulty, always all 4 ports that fail.
The failing units have mainly been supplied from a solar/battery power source and our testing has revolved around repetitive charge/discharge cycles providing significant power cycles of the PSE but this hasn't shown any problems.
Any suggestions as to the failure mode.