TPS653860-Q1: Comparator module

Part Number: TPS653860-Q1

Tool/software:

Dear Support Team,

we're looking for the possibility to monitor an external voltage with the reference of 2.4V by the Comparator Module (CM).

The electrical characteristic POS 27.1.8 shows a VMON_REF=0.6V and we understand that this reference voltage is valid for the configuration COMPx_CFG = 110b (= both inputs in voltage monitor mode).

The blockdiagram (Fig. 8-53) of the CM shows that either 0.6V or 2.4V can be selected.

In case we configure COMPx_CFG = 101b (= single ended comparator, 2.4V (typ) reference, inverting input in voltage monitor mode) what will be the reference voltage of the monitor ?

is there a more detailed  information/application note for the Comparator Module than given in the datasheet?

Thanks in advance.

Best regards,

Andreas