Tool/software:
Dear support,
I have a couple of questions regarding the output leakage currents specified in the datasheet, specifically I(ol,off) and Ilkg(out), which are defined under different conditions.
- I(ol,off) is sinking -75 uA (current flowing into the pin OUTx) under conditions VINx = 0 V, VDIAG_EN = 5 V, VVS = VOUTx = 13.5 V, TJ =125°C, open load
- Ilkg(out) is specified as +0.5 µA (current flowing out of the OUTx pin) under the following conditions: VVS = 13.5 V, VINx = VDIAG_EN = VOUTx = 0 V
That suggest that the state of VDIAG_EN might affect the leakage current value.
1) Could you please clarify the value of I(ol,off) when VDIAG_EN = 0 , while keeping the other conditions the same?. Does I(ol,off) decrease (in absolute value) in this scenario?
2) I would also like to know the value of I(ol,off) at different temperatures and VOUTx levels.
Thank you for your support
Best regards
Joaquin Fernandez