Tool/software:
Team,
My customer has a question about the lifetime of the LM78L05ACMX/NOPB. The device needs to be operated in a fast ON/OFF condition (see below for details). The engineers would like to know if this behaviour causes the short lifetime or early ageing. Could you please comment on this? Thanks!
Vin = 24 V
Vo = 5 V
Load = less than 20 mA
ON/OFF = 50 Hz with 50% duty cycle.
Regards,
Sam Ting