Tool/software:
Can I use a TMUXHS221F (USB/UART switch) to mux the CC1 and CC2 lines of 2 USB-C connectors to a TPS25751S? The USB-C connections are for attachment of a 60W USB-C PD source. One connection is supplied from a docking station, the other is simply a convenience connection USB-C port. The docking station would be the default source. The secondary port would allow a PD source to be connected if the docking station was unavailable. The USB-C data lines are not used the connections are used to negotiate a 12V 5A supply from the PD source.