BQ25306: STAT Pin is toggle

Part Number: BQ25306

Tool/software:

Hi. 

BQ25306 was used to design a standalone charger.

The STAT pin is toggles to 1HZ.

* TS pin

  -. The TS pin was entered at 1.2V by replacing the R17 and R21 resistors for testing. R20 is NC

* VBUS 

  -. The voltage of the VBUS is 5V. It is powered by a USB charger.

* EN

  -. The EN pin is connected by a 10K pull-down,

* POL 

  -. POL pin is floating.

* BAT

  -. When the battery is connected to P2, the BAT pin  Voltage measures 3.7V.

* REGN

  -. REGN pin output 5V 

* SW

  -. The SW pin is connected to a 1uf inductor and when the VBUS voltage is connected, the STAT pin toggles. 

     At this time, 0.7V is measured when the SW pin voltage is measured

 -. 3.7V (battery voltage) is measured when measuring the SW pin when the battery is connected to P2.

The problem is that the STAT pin keeps toggling.

I don’t' know the reason.