Tool/software:
Hello,
The customer uses the INTEL ADL-2 platform and requires a PD chip for TPC interface connection to Type-C. The packaging requirements are smaller, with a current of 1A sufficient and no external charging. The main purpose is to perform CC detection and signal switching. The customer is interested in TPS65994AERSLR, but this chip is not recommended for new designs. Therefore, TPS26750 is recommended. May I ask if TPS26750 can meet the requirements, whether it is compatible with Intel ADL-N platform, or if you can help recommend a better solution? Thank you!