Other Parts Discussed in Thread: BQ25606
Tool/software:
hello all,
i was looking at the EVB of BQ25606, and im trying to charge a battery which voltage is at 3.6V.
But i got an issue, i see that the current is fixed at 2A ( the charging current ) and i cant get why, consider that ILIM and ICHG has lowest resistor possible,
So 158 Ohm for ILIM and 221 Ohm for ICHG, i also removed from the board R23 which was a resistor in parallel to R24 ( 10k Ohm ) but nothing changed, in theory with a resistor of 10kohm to gnd it means that at normal temperatures i will have highest charging current.
what else i could try to do?