TPS92682-Q1: CHxUV fault

Part Number: TPS92682-Q1

Tool/software:

Hi team,

My customer is evaluating TPS92682-Q1 in their project and met below issue, could you help give some comments?

In CC mode, CHxVU is set to 1 in the FLT register when the output is shorted to ground.

When the customer removes the short circuit, the customer rereads this register at intervals of 10ms per cycle. In the fifth cycle(50ms), CHxUV=1 can still be read even if the fault is cleared. And CHxUV is cleared to 0 at the seventh cycle(70ms) .

Is this a reasonable phenomenon? Why is it so long before CHxUV is cleared 0? Thanks.

Thanks.

Regards,
Ivy