LM74610-Q1: Compatible MOSFET with LM74610-Q1

Part Number: LM74610-Q1
Other Parts Discussed in Thread: TPS92638-Q1,

Tool/software:

Hello,

We are working on design of LED driver to drive 6 LEDs in parallel (each with 11mA current, Vf 2.8V). we have decided to use TPS92638-Q1 for the same. For making the design compliant to automotive test cases - planning to include LM74610-Q1 between input supply of battery and LED driver IC.

To connect N-channel mosfet, we are planning to use the part RSR025N05HZG. (MOSFETS suggested in LM74610-Q1 are all high current and hence size is more. we are looking at load current of 1A only. so please let us know if RSR025N05HZG is compatible N-channel MOSFET to use with LM74610-Q1.

This is critical to finalize component selection. Awaiting for your quick confirmation regarding this.

Thanks,

Smitha R