Other Parts Discussed in Thread: LM51770, PMP23377
Tool/software:
Hi, TI's experts
I have a design task that input range is : 9 - 40V voltage input, 1kW power output with 12V voltage, which means a more than 80A output current.
So I have to find a chip can output 20A current and can be config work in multiphase parallel. then I find LM51772, whcih is a buck-boost controller with extenal MOS and can work in parallel.
But, I can only find the LM51772 work in 2 parallel chip, in that case, the board can not deliver a 1kW output power. It need 4 chip work in parallel can deliver a 1kW power with good thermal condition. in my opinon
So, my question is, can LM51772 work in 4-chip parallel to deliver a 1kW power. If can't, what else choice can I have