LP8865Z-Q1: Working junction temperature

Part Number: LP8865Z-Q1

Tool/software:

Hello, I saw in the specification sheet that the working environment temperature is 125℃ and the maximum junction temperature is also 125℃. Are there any conflicts between these two? Because in an environment of 125℃, the chip will have a temperature rise when working, or does it mean that the junction temperature of this chip is higher? Can it reach up to 150℃ at most?